2007-03-07 5:52 AM
2007-03-07 2:44 AM
Could ST confirm the following:
In the function RCCU_PLL2Config the FRQRNG bit should be set if the freq is above 3MHz. PCU->PLL2CR = ( Tmp & ~RCCU_DX_Mask ) | ( New_Div | RCCU_FREEN_Mask ) | 0x40; I also have a query with RCCU_PLL1Config: This function seems to set the FREEN bit for frequencies above 3MHz, surely this should be setting the FREF_RANGE instead and always setting the FREEN bit. Regards sjo2007-03-07 5:52 AM
Hello Sjo,
Thanks for your inputs: 1- We confirm, in the function RCCU_PLL2Config the FRQRNG bit should be set when the PLL input frequency ''HCLK pin'' is in the range 3-5 MHz as specified in the reference manual. 2- Regarding the RCCU_PLL1Config function, we totally agree. For input frequency ''CLK2'' greater than 3MHz, the FREF_RANGE bit should be set rather than the FREEN bit. All these issues should be fixed in the next release of software library. Thanks.