cancel
Showing results for 
Search instead for 
Did you mean: 

STR711 UART baudrate

victor2399
Associate II
Posted on April 30, 2006 at 07:32

STR711 UART baudrate

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
victor2399
Associate II
Posted on April 27, 2006 at 13:38

Hi.

I'm using STR711-SK board, connected via ULINK.

I use code from example for setting baudrate 9600.

But I get baudrate 2400.

Here is my code, please advice where the problem can be.

Thanks.

GPIO_Config(GPIO0, UART0_Tx_Pin, GPIO_AF_PP);

GPIO_Config(GPIO0, UART0_Rx_Pin, GPIO_IN_TRI_CMOS);

UART_Init(UART0);

UART_OnOffConfig(UART0, ENABLE);

UART_FifoConfig (UART0, DISABLE);

UART_FifoReset (UART0 , UART_RxFIFO);

UART_FifoReset (UART0 , UART_TxFIFO);

UART_LoopBackConfig(UART0 , DISABLE);

UART_Config(UART0,9600,UART_NO_PARITY,UART_1_StopBits,UARTM_8D);

UART_RxConfig(UART0 ,ENABLE);

EIC_IRQChannelPriorityConfig(UART0_IRQChannel, 1);

EIC_IRQChannelConfig(UART0_IRQChannel, ENABLE);

EIC_IRQConfig(ENABLE);

UART_ItConfig(UART0,UART_RxBufFull, ENABLE);

UART_ByteSend(UART0, ''d'');

victor2399
Associate II
Posted on April 27, 2006 at 13:59

I have changed it already to 4000000, but if I play with this value I see no changes. More ideas?

victor2399
Associate II
Posted on April 28, 2006 at 19:28

Hi, thanks for reply.

I haven't changed the clock configuration. It is default after reset. Just as in example ''UART'' from ST. Code that you see thats all.

victor2399
Associate II
Posted on April 30, 2006 at 07:32

I have recompiled the library from source. Now all working fine.