cancel
Showing results for 
Search instead for 
Did you mean: 

I2C Problem - STR710 + ST0676

ckirmse9
Associate II
Posted on May 01, 2006 at 11:05

I2C Problem - STR710 + ST0676

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ckirmse9
Associate II
Posted on April 21, 2006 at 09:57

Hallo,

I am trying to get a ST0676 connected to a STR710 working.

The first time I read for instance, the Version register of the ST0676

everything is ok, but on the second access the read bit in the address is always set.

I use the STR7x Library and the following code:

void I2cInit(I2C_TypeDef *I2Cx, int Clock)

{

I2C_Init(I2Cx);

I2C_FCLKConfig (I2C0);

I2C_OnOffConfig (I2C0, ENABLE);

I2C_SpeedConfig (I2C0, Clock);

I2C_AddressConfig (I2C0, 0x0C0, I2C_Mode7);

I2C_AcknowledgeConfig (I2C0, ENABLE);

}

int I2cRead(I2C_TypeDef *I2Cx, int cmdLen, int readLen, unsigned char *bufp)

{

I2C_Tx_Status sendaddress,bSendResult;

I2C_Rx_Status rxStatus;

int i, I2CStatus;

I2cInit(I2Cx, 4000);

I2C_STARTGenerate(I2Cx, ENABLE);

while(I2C_FlagStatus(I2Cx, DIRECT, I2C_SB ) == RESET);

I2C_AddressSend(I2Cx, bufp[0], I2C_Mode7, I2C_TX);

//Test on the status of transmission

while(sendaddress != I2C_TX_ADD_OK) {

sendaddress = I2C_TransmissionStatus(I2Cx);

}

while(I2C_FlagStatus(I2Cx, DIRECT, I2C_ENDAD) == RESET);

I2C_FlagClear(I2Cx, I2C_ENDAD);

for(i = 1; i < cmdLen; i++) {

I2C_ByteSend(I2Cx, bufp[i]) ;

//Test on the status of transmission

while(bSendResult != I2C_TX_DATA_OK) {

bSendResult = I2C_TransmissionStatus(I2Cx);

}

}

//Stop the transmission

I2C_STOPGenerate (I2Cx, ENABLE);

// delay for the ST0676

ctl_timeout_wait(DELAY(10));

I2C_STARTGenerate(I2Cx, ENABLE);

while(I2C_FlagStatus(I2Cx, DIRECT, I2C_SB ) == RESET);

// send register address

I2C_AddressSend(I2Cx, bufp[0], I2C_Mode7, I2C_RX);

//Test on the status of transmission

while(I2C_FlagStatus(I2Cx, DIRECT, I2C_ENDAD ) == RESET);

I2C_FlagClear(I2Cx, I2C_ENDAD);

for(rxStatus = 0, i = 0; i < readLen - 1; i++) {

//Test on the status of transmission

while(rxStatus != I2C_RX_DATA_OK) {

rxStatus = I2C_ReceptionStatus(I2Cx);

}

// get the byte received

bufp[i] = I2C_ByteReceive(I2Cx);

}

// receive last byte

I2C_AcknowledgeConfig (I2C0, DISABLE);

bufp[i] = I2C_ByteReceive(I2Cx);

i++;

//Stop the transmission

I2C_STOPGenerate(I2Cx, ENABLE);

I2C_OnOffConfig(I2Cx, DISABLE);

return i;

}

I hope there is anybody who give me and idea what’s wrong.

Regards,

ctk

ckirmse9
Associate II
Posted on May 01, 2006 at 11:05

Hi,

in the mean time i found the problem (or get close to). The ST0676 is very slow.

To compensate this I have inserted several delays in the I2C read part.

But the communication between the STR10 and the ST0676 is very unstable.

The main Problem is a Arbitration Lost Error (in case of a write cmd) in the Status of the I2c-status register,

which only should occur in a multi master environment, but the both devices are the only one on the bus. The bus is pulled up with 4k7 Resistors (I also tried other values with no

different). Did you have any idea what the reason for this status (ARLO) is ?

regards, ctk