STR710Lib mapping in the apb.h file is not correct ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2005-08-24 5:23 AM
Posted on August 24, 2005 at 14:23
STR710Lib mapping in the apb.h file is not correct ?
Labels:
- Labels:
-
Legacy Products
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2005-08-24 5:23 AM
Posted on August 24, 2005 at 14:23
I think the correct mapping for the APBn_SWRES and APBn_CKDIS registers in the apbh.h file of the STR710Lib must be
/* APB1 Peripherals */ #define I2C0_Periph 0x0001 #define I2C1_Periph 0x0002 #define UART0_Periph 0x0008 #define UART1_Periph 0x0010 #define UART2_Periph 0x0020 #define UART3_Periph 0x0040 #define USB_Periph 0x0080 #define CAN_Periph 0x0100 #define BSPI0_Periph 0x0200 #define BSPI1_Periph 0x0400 #define HDLC_Periph 0x2000 /* APB2 Peripherals */ #define XTI_Periph 0x0001 #define GPIO0_Periph 0x0004 #define GPIO1_Periph 0x0008 #define GPIO2_Periph 0x0010 #define ADC12_Periph 0x0040 #define CKOUT_Periph 0x0080 #define TIM0_Periph 0x0100 #define TIM1_Periph 0x0200 #define TIM2_Periph 0x0400 #define TIM3_Periph 0x0800 #define RTC_Periph 0x1000 #define WDG_Periph 0x2000 #define EIC_Periph 0x4000 and not /* APB1 Peripherals */ #define I2C0_Periph 0x0002 #define I2C1_Periph 0x0004 #define UART0_Periph 0x0010 #define UART1_Periph 0x0020 #define UART2_Periph 0x0040 #define UART3_Periph 0x0080 #define USB_Periph 0x0100 #define CAN_Periph 0x0200 #define BSPI0_Periph 0x0400 #define BSPI1_Periph 0x0800 #define HDLC_Periph 0x2000 /* APB2 Peripherals */ #define XTI_Periph 0x0002 #define GPIO0_Periph 0x0004 #define GPIO1_Periph 0x0008 #define GPIO2_Periph 0x0010 #define ADC12_Periph 0x0080 #define TIM0_Periph 0x0200 #define TIM1_Periph 0x0400 #define TIM2_Periph 0x0800 #define TIM3_Periph 0x1000 #define RTC_Periph 0x2000 #define WDG_Periph 0x4000 #define EIC_Periph 0x8000 as in the actual version (V3.0) of the Str710Lib these mapping is used in the APB_SwResetConfig and APB_ClockConfig calls.