2007-01-09 2:56 AM
str710fz2 Programming by RIDE error
2007-01-06 12:49 AM
Hi,
I am using RIDE BN version 746 & RFlasher to program STR710FZ2. I was able to program so far. I am booting from internal FLASH, using ST libraries. 1. Today it started giving message like ''Timeout Expired while Trying to reset Target'' for any commands like erase, blankcheck etc. But it can communicate with target & reads device id. Why is it? 2. I have enabled UART3's TxEmpty interrupt and it is doing transmission fine(continuously). I am using ST library functions to init or configure device. But I am getting non-stop TxEmpty interrupts even if i dont write anything to TxBUFR register. I even trying to clear pending bit with '1' but of no use. 3. I am using EMI BANK0 to connect to CompactFlash but not yet soldered CF. If I only read, i dont see any RDn or CS0 signal on scope but if add some write instruction, i can see both RDn, WRn, CS0. Why is it? Please help. Thanks in advance.. :-[2007-01-09 2:56 AM
Hi,
I answered the first question on the Raisonance forum: http://www.raisonance.com/Forum/phorum-3.3.2b2/read.php?f=1&i=6822&t=6822 I don't know the answers to the two other points... Best Regards, Vincent