cancel
Showing results for 
Search instead for 
Did you mean: 

STR7-RVDK && IAR STR711 KickStart

shlomotz1
Associate II
Posted on October 16, 2006 at 11:20

STR7-RVDK && IAR STR711 KickStart

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
shlomotz1
Associate II
Posted on October 16, 2006 at 08:13

Hello,

I’m using the STR7-RVDK with the STR7 Eval Board MB393.

Can I use the same tools with IAR STR711 KickStart Board?

Thanks,

Shlomo

tech9
Associate II
Posted on October 16, 2006 at 11:20

I believe you can. Toolsets are supposed to be transparent. However I did that using the IAR tool; works perfectly on both boards (MB393 with a STR710, and KickStart with a STR711).

All you need to do is to change some defines for the PLL base frequency (crystals are different, one is 4 MHz and the other is at 16MHz), change the supply (one is powered through the JTAG link) and you're good to go.

Some people might want to confirm the exact procedure for your toolset... Anyone?

Hope this helped you a little

Jp