2025-03-14 5:31 AM - last edited on 2025-03-14 6:23 AM by Andrew Neil
Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2).
STM32IDE (1.18.0) for the STM32F103C8T6 always fails to start the GDB after download and installation, and there is no method on the web page or official manual. Recent successes are STM32IDE (1.17.0) still working in mid to early February, and STM32IDE (1.17.0) not working at the end of February. (ST-link V2 to STM32F103C8T6)
Original:
3C8T6M32F的STM32IDE (1.18.0) 下载安装后总是无法启动 GDB,网页上的方法和官方手册也没有。最近的成功是 STM32IDE (1.17.0) 在 2 月中旬到初仍在工作,而 STM32IDE (1.17.0) 在 2 月底无法正常工作。(ST-link V2 to STM32F103C8T6)
Solved! Go to Solution.
2025-03-17 8:47 AM
Are you sure that it actually works out cheaper than buying a Nucleo board - which includes a genuine ST-Link?
A Nucleo-103 is under £10 !
So long as you're aware that you are using fake/clone gear - and the many difficulties that may cause.
Again, see this thread for the grief the fakes can cause ...
And, of course, you can't count on support from ST!
2025-03-17 8:55 AM
Are you sure you have that wiring correct?
2025-03-17 9:39 AM
swd -- swc puzzled . :D
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.