cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 (Blue Pill): Dual/Synchronous ADC Mode Fails on Real Hardware, Works in Proteus Simulation

Rafsan_BD
Associate

Dear Embedded Community,

I am facing a persistent and frustrating issue concerning the Dual ADC Synchronous Multi-Channel Mode on my Blue Pill board (STM32F103C8T6). The setup works perfectly in simulation but fails completely on the actual physical hardware.

I'm seeking guidance on how to confirm the functional integrity of the ADC2 peripheral on this specific board.


 

1. Hardware & Software Setup

 

  • Microcontroller: STM32F103C8T6 (Blue Pill - likely a clone/fake chip).

  • Development Environment: STM32CubeIDE / HAL Library (latest F1 series version).

  • ADC Configuration: Dual Regular Simultaneous Mode (Synchronous Multi-Channel).

    • ADC1 Channels: CH0 and CH1 (Injected/Regular, typically triggered by a Timer).

    • ADC2 Channels: CH2 and CH3 (Running as the Slave, triggered by ADC1).

    • Transfer Method: DMA (Circular Mode) to a single buffer.


 

2. The Problem: Simulation vs. Reality

 

My goal is to sample two pairs of analog signals simultaneously (true synchronized reading).

ScenarioExpected Output (ADC Buffer)Actual Result on Hardware
Proteus SimulationAlternating, synchronized data from ADC1 (CH0/CH1) and ADC2 (CH2/CH3). Success. 
Real Blue Pill HardwareIncorrect/stuck data for ADC2 channels. Often, the DMA buffer only shows the mirrored data of ADC1, or ADC2 data is consistently zero/stuck at a random value. Failure. 
Testing ADC2 AloneWhen running only ADC2 in Single/Scan Mode (not Dual Mode), it reads its designated channels (CH2/CH3) correctly. 

The root issue is that ADC2 is not being correctly triggered or synchronized by ADC1 in the Dual/Synchronous Mode.


 

3. My Hypotheses & Context

 

Based on community knowledge, I suspect two possibilities:

 

Hypothesis A: The Fake Chip Problem

 

It is well-known that many Blue Pill boards contain fake/cloned chips (e.g., CKS32, GD32, or chips with unreliable ID markings). While the chip may have the ADC2 peripheral, the complex synchronization logic required for Dual Mode may be poorly implemented or non-functional in the clone's silicon, causing the trigger failure. Proteus assumes a perfect ST chip, while the real hardware is flawed.

 

Hypothesis B: F103 Hardware Quirks

 

The original STM32F103 is an older design with known ADC synchronization complexities. I am aware that:

  1. Only the ADC1 DMA request is used for Dual Mode.

  2. Specific control bits (even those seemingly unrelated) need to be set to enable the ADC2 data mirror/triggering on ADC1's register. It's possible the HAL implementation is missing a crucial register setting for the F103 to correctly activate the ADC2 slave trigger.


 

4. Specific Question to the Community

 

  1. Has anyone successfully implemented Dual Simultaneous Regular Mode (Synchronous Mode) on a cheap Blue Pill board? If so, what specific bare-metal register settings (outside of the CubeIDE HAL) were required to ensure ADC2 is correctly triggered by ADC1?

  2. Is there a reliable way to confirm the Device ID or internal silicon revision of the STM32F103C8T6 chip to determine if I am dealing with a known clone lacking full ADC functionality?

Any insights, especially those addressing the specific ADC2 triggering logic in the F103's common registers, would be highly appreciated.

Thank you in advance for your time and expertise!

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Blue/Black pill boards contain F103 contrefeit products and most probably it's the case for you.

So we suggest to purchase one of the Nucleo board having genuine STM32 MCUs. like NUCLEO-F103RB.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
mfgkw
Senior III

Hi Rafsan,

 

Meanwhile the chance to have a genuine STM32 on a blue pill is really low (assuming your board is not one the really early ones).

I have some naked STM32F103RBT6 here (without any PCB around). If your project needs no specific environment (besides ST-Link and maybe some UART or some resistors) or if you can strip it down this way I could run it on an programming adapter and see how it behaves on an original STM32.

 

But my recommendation is to buy a NUCLEO board for some € or $ and use this for testing.

mƎALLEm
ST Employee

Hello,

Blue/Black pill boards contain F103 contrefeit products and most probably it's the case for you.

So we suggest to purchase one of the Nucleo board having genuine STM32 MCUs. like NUCLEO-F103RB.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

“Thanks for your suggestion. In our market, the STM32 NUCLEO-F103RB Development Board – STM32F103RBT6, ARM Cortex-M3, 128KB Flash, 20KB SRAM is available. What can be done with this model?


@Rafsan_BD wrote:

What can be done with this model?


Many things to do as the board exposes most of the MCU GPIOs externally on the available connectors.

You can start by running examples from CubeF1 software package: https://github.com/STMicroelectronics/STM32CubeF1/tree/master/Projects/STM32F103RB-Nucleo

More advanced applications here: https://github.com/STMicroelectronics/STM32CubeF1/tree/master/Projects/STM32F103RB-Nucleo/Applications

You can also find many tutorials on youtube that demonstrate ADC examples. Google "stm32f103 nucleo ADC demo". 

Hope that helps

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Andrew Neil
Super User

@Rafsan_BD wrote:

3. My Hypotheses & Context

Based on community knowledge, I suspect two possibilities:


A third possibility, of course, is that your Proteus simulation does not match your actual hardware.

That could be due to:

  • Errors in your Proteus setup
  • Errors in your physical setup
  • Limitations in Proteus simulation
  • some combination of the above

Simulations tend to assume ideal components and conditions ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.