2004-06-08 8:48 AM
STDV3.0 - WatchWindow - Expanding the display
2004-06-07 11:14 AM
Using STDV3.0, I want to see an array that is 32 bytes long.
In the 'WatchWindow' when I click on the '+' sign in order to 'Expanding the display' (as described in the user manual), I can only see the first 10 elements of the array. If I want to see more, I have to go to the 'memory window' and scan through it in order to see all the data. My question is: Is there a way to expand an array (bigger than 10 elements) up to its end in the 'WatchWindow'?2004-06-08 12:18 AM
Same process as older 2.54 - goto Tools/Options/Edit Debug modify Watch array expand ** items to suit.
Regards sjo2004-06-08 8:48 AM
Works just marvellously.
Thanx sjo.