2005-09-15 4:56 PM
static or dynamic RAM in ARMSTR7?
2005-09-15 12:03 AM
Hi,
I would like to know if the 64Kbytes of RAM is in dynamic or static form. Rgrds, ongth602005-09-15 4:56 PM
Hi guys,
Thanks for the answer. If the CPU resets, will the variables declared in RAM able to retain the value long enough cos I've a watchdog to reset the CPU in case if the program hangs? Rgrds, ongth60