2006-02-27 5:03 AM
ST7Ultralite : Amazingly small ... tremendously useful !
2006-02-14 8:19 PM
Hello,
I'm happy to announce you that our new ST7Ultralite is now available. This is a 8-pin chip working from 2.4v to 5.5v, embedding : - an internal RC 8MHz oscillator, - an auto wake-up 33kHz oscillator, - with low voltage detection capabilities, - 1k of single voltage Flash programming memory. - a 12-bit Auto Reload Timer with output capture and PWM, - a 8-bit Timer with watchdog, - a 10-bit A/D converter (up to 5 channels), - 6 I/O lines (5 with High Sink capabilities), - 5 power saving modes, - available in DIP8, SO8 and DFN8 packages, - less than 16 mm² in DFN8. This is a small micro bursting with features. You can find all the detailed information by searching for ''ultralite'' in the ''Search ST MCU'' field or by having a look to the official press release :http://www.st.com/stonline/stappl/press/news/year2006/p1768.htm
Feel free to ask your questions in this forum. Best regards Laurent2006-02-21 1:31 PM
HI
HOW R U .HOPE FINE . I AM CONCERNED WITH HOW TO INCIRCUIT PROGRAM THE MICRO ST7ULTRALITE WITH THE USB STVD7-INDARTSTX- . THE KIT DOESN'T SUPPORT IT IN ITS DEVICES .SO HOW CAN I PROGRAM IT ? I TRIED THE ST7FLIE0 CNFIGURATIIONS , IT DOESN'T WORK SO CAN YOU PLEASE ADVISE ME OF HOW TO PROGRAM THIS AMAZINGLY SMALL BUT TRMENDOUSLY USEFUL MICRO. :D2006-02-24 8:38 AM
Hy,
You have forget to say that this ST7ultralite MCUs have the same shape of microchip PIC10xxx ( EEPROM included! ) and freescale MC68HC908QTx!! By2006-02-27 5:03 AM
Hello,
The IndartSTX will be soon available. I will update this post as soon as i get a date. BR Laurent