cancel
Showing results for 
Search instead for 
Did you mean: 

ST7Lite - Internal RC with RS232

asherman
Associate II
Posted on July 23, 2003 at 12:43

ST7Lite - Internal RC with RS232

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
asherman
Associate II
Posted on May 19, 2003 at 07:53

Hello All ,

I want to use the ST7Lite05 with the Internal RC oscillator and to work with the SCI (RS232) communication .

Do you think that there will be a problem with the communication in several computers because of the accuracy or not ?

Shermantec
itsmejatinus
Associate II
Posted on May 19, 2003 at 11:54

Internal RC has an accuracy of 1% as specified into the datsheet.

sisto
Associate II
Posted on July 22, 2003 at 13:31

With RC clock You will have bit sample problems during a receiver session, with higher baud rates. I have used this solution with satisfaction for baud rates lower than 2000 bps.

simonharrison9
Associate II
Posted on July 23, 2003 at 08:55

Hi,

I'm running at 9600 with no problem.

The only risk is when the supply changes,as this will change the clock freq.

Simon

Anglia
itsmejatinus
Associate II
Posted on July 23, 2003 at 12:43

I have tested it from 2.4kbps to 19.2kbps without any problem with internal RC clock.