2007-06-13 10:36 PM
2007-06-12 3:31 AM
Hi,
I'm in front of a problem by the using of a function which should give the checksum of my software. #ifdef USE_HDFLASH_CHECKSUM /*----------------------------------------------------------------------------- ROUTINE NAME : HDFlashChecksum INPUT : Flash address, Frequency OUTPUT : Embedded Command Status Returned values of Checksum are in EMBLG_PARAM_ENDH and EMBLG_PARAM_ENDL addresses DESCRIPTION : Compute a Checksum -----------------------------------------------------------------------------*/ unsigned char HDFlashChecksum(unsigned char *Flash, unsigned char Freq) { EMBLG_PARAM_ECMD = 0x06; EMBLG_PARAM_PTRL = ((int)Flash & 0xFF); // Flash Address Low Byte EMBLG_PARAM_PTRH = ((int)Flash >> 8); // Flash Address High Byte EMBLG_PARAM_FREQ = Freq; FCSR = 0x00; // Launch command (no need to wait end of operation) return EMBLG_PARAM_ECMD; // Return Embedded Command Status } #endif How can I know the ''Flash Address Low Byte'' of my soft? So what should be the value of ''Flash''? thanks for your help2007-06-13 10:36 PM
Hi,
although I don't really comprehend your problem in detail, I'll try to give some ideas. Declaring the EMBLG_PARAM_PTR as pointer to an unsigned character with char *EMBLG_PARAM_PTR;you'll get the two byte number EMBLG_PARAM_PTR as pointer to an unsigned char. To calculate the checksum you only have to add all the values of your flash from the first to the last byte. checksum = 0;for(EMBLG_PARAM_PTR = FLASH_FIRST_BYTE; EMBLG_PARAM_PTR <= FLASH_LAST_BYTE;) checksum += *(EMBLG_PARAM_PTR++);where FLASH_FIRST_BYTE and FLASH_LAST_BYTE are constant pointers to the first and to the last byte of your flash. But pay attention: If FLASH_LAST_BYTE == 0xFFFF you'll meet a serious problem: Increasing EMBLG_PARAM_PTR (== 0xFFFF) causes an overrun to 0x0000. Then the query EMBLG_PARAM_PTR <= FLASH_LAST_BYTE will give a wrong result and you might enter a deadloop!!! In this case better use checksum = 0;
for(EMBLG_PARAM_PTR = FLASH_LAST_BYTE; EMBLG_PARAM_PTR >= FLASH_FIRST_BYTE;) checksum += *(EMBLG_PARAM_PTR--);Alternatively to declared constants you might take numerical constants as addresses: checksum = 0;
for(EMBLG_PARAM_PTR = (unsigned char*)0xFFFF; EMBLG_PARAM_PTR >= (unsigned char*)0x8000;) checksum += *(EMBLG_PARAM_PTR--);Hope it will help you to find a solution, WoRo