2006-07-13 6:51 AM
2006-07-12 10:30 AM
The datasheet for this device gives details for 4 option bytes, yet the Visual Programmer only has settings for three.
Could ST clarify this situation, also does this device have a backup oscillator as per the datasheet ? Regards sjo2006-07-12 10:10 PM
Hi,
As you can read in the datasheet all bits of option byte #2 are reserved, so there is no need to access it ! It is why STVP7 only provide a way to read/write only 3 option bytes. You should have get a preliminary datasheet and there was a mistake as there is no backup oscillator in the ST72F344. Best regards Laurent2006-07-12 10:14 PM
The CSS is mentioned in STVP7 ?
Regards sjo2006-07-13 6:51 AM
CSS will be removed in the next release, it was a mistake !
Thanks for your feedback ! Best regards Laurent