cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 Programming Error

oc
Associate II
Posted on August 21, 2008 at 14:57

ST7 Programming Error

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
oc
Associate II
Posted on May 23, 2008 at 09:11

Hello,

I am using an ST72F60E1 device, trying to program through an RLINK USB programmer.

I've actually had this working before, but coming back to it after a few months and now I'm getting this error:

''Error : Cannot communicate with the device ! Option Bytes are Enabled on the device.

Check the ICC cable connection and check all the needed pin connections on the ICP connector.''

I've double- and triple-checked the ICC connections, and I'm sure they're correct. I'm using a 12MHz crystal on the board, which is producing a steady clock. The application power supply is 5v from the USB bus.

What are the possible sources of this error? It must be something simple...

silicon
Associate II
Posted on May 26, 2008 at 06:47

Hi

You can try to change booten bits set to load from external (1,1,1).Then erase flash and set booten to load from flash (0,0,0).

r,A

oc
Associate II
Posted on May 27, 2008 at 07:23

OK, how do I do that? I am using ST7 Visual Programmer.

sjo
Associate II
Posted on May 27, 2008 at 12:08

Afraid you don't, silicon.ray is confusing your device with the strxx family.

Normally just check your have the latest version of Visual Programmer

Could also try checking the reset line for to much capacitance.

Are the ICC line shared with your application?

Cheers

sjo

oc
Associate II
Posted on August 21, 2008 at 14:57

I am using the latest version of ST7VP/ST7VD, the reset line has no capacitance (that was a problem before), and the ICCDATA/ICCCLK are not shared by the application.

Having tried the RLINK with another board and MCU, that's not working either, so maybe I've somehow damaged the programmer...