cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 BE USED FOR A RS232

asherman
Associate II
Posted on May 27, 2003 at 15:08

ST7 BE USED FOR A RS232

3 REPLIES 3
asherman
Associate II
Posted on May 22, 2003 at 10:13

Hello

CAN ST7 BE USED FOR A RS232 COMMUNICATION WHEN USING INTERNAL RC OSC. ?

IS THERE ANY APPLICATIONS FOR IT?

WE NEED BAUD RATE OF 2400.

I WOULD LIKE TO ADD THAT THE COMMUNICATION IS BETWEEN PC TO MY DEVICE.

Shermantec

itsmejatinus
Associate II
Posted on May 22, 2003 at 11:01

Yes, there is an application note available for it i.e. AN1530.This application note calliberates the SCI parameter w.r.t internal RC variation.This AN ia valid for the micros which have SCI inbuilt.

There is an another AN 973 (SCI Software Communication with a PC Using ST72251 16-Bit Timer) in case SCI peripheral is not available.

For Lite, internal RC has 1% tolerance, but SCI peripheral is not available.
stephanie
Associate II
Posted on May 27, 2003 at 15:08

A RS232 software driver dedicated to litex is under writing and will be soon availble!