Skip to main content
john8
Associate
December 10, 2003
Question

st626x starter kit

  • December 10, 2003
  • 2 replies
  • 820 views
Posted on December 10, 2003 at 07:37

st626x starter kit

This topic has been closed for replies.

2 replies

john8
john8Author
Associate
December 8, 2003
Posted on December 08, 2003 at 12:41

When trying to program st6265 with the starter kit and Intel hex code generated by Realizer 2 I am receiving verify error message at address 0080. Previously have successfully programmed chips with the same code and starter kit but on a different computer.My prenet computer is a laptop. Can successfully read from chips and blank check and verify but cannot verify when hex file is opened or program the chip. Has anyone any bright ideas?

THE PROBLEM WAS SIMPLY THAT THE VOLTAGE I WAS USING (12V) WAS BELOW THE RECOMMENDED VALUE OF BETWEEN 16-20V. SIMPLE MISTAKE BUT BEWARE!

[ This message was edited by: jaycee on 12-12-2003 16:51 ]
vikas2
Visitor II
December 10, 2003
Posted on December 10, 2003 at 07:37

The starter kit compatibility upto some extent depend on PC to PC. The problem in your case could be because of high speed of your Laptop. Also use the latest verion of Window eprommer (Winee 4.0.3) and then try. It is free available on internet(www.stmcu.com).