cancel
Showing results for 
Search instead for 
Did you mean: 

SPI read problem

tj2
Associate II
Posted on October 11, 2005 at 15:17

SPI read problem

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
tj2
Associate II
Posted on October 10, 2005 at 13:08

Hi

I'm running a FRAM as a slave on the SPI bus (BSPI1). I got a problem when reading from the bus or more precisely the receive buffer. The data is perfectly clocked out of the FRAM, but when reading the receive buffer I get a wrong value (0x00). When I dump the memory at 0xC000B000 (BSPI1) the correct value is in the buffer.

When single stepping through the read routine, it works perfectly. I've tried to use both the ReceiveFifoNotEmpty and ReceiveFifoFull flag, but this does not help.

Below is my code. I hope someone can help...

Main routine:

_________________________________________

GPIO_Config (GPIO0, 0x0010, GPIO_AF_PP);

GPIO_Config (GPIO0, 0x0020, GPIO_AF_PP);

GPIO_Config (GPIO0, 0x0040, GPIO_AF_PP);

BSPI_Init ( BSPI1 ); // Initialize BSPI1

BSPI_ClockDividerConfig ( BSPI1,8); // Configure Baud rate Frequency :-->APB1/8

BSPI_Enable ( BSPI1 , ENABLE ); // Enable BSPI1

BSPI_MasterEnable ( BSPI1,ENABLE ); // Configure BSPI1 as Master

BSPI_ClkActiveHigh(BSPI1,DISABLE); // Configure the clock to be active low

BSPI_ClkFEdge(BSPI1,DISABLE); // Disable capturing the first Data sample on the first edge of SCK

BSPI_8bLEn(BSPI1,ENABLE); // Set the word length to 8 bit

FRAM_StatusReg=framReadStatusReg();

Read Status Register Routine:

_________________________________________

u8 framReadStatusReg() {

u8 dummy;

Latch1_BitWrite(LATCH_CS_FR,0); // Select device

while(BSPI1->CSR2&BSPI_RFNE) dummy = BSPI1->RXR; // Clear the RX Fifo.

while(!(BSPI1->CSR2&BSPI_TFE)); // Wait until the Transmit FIFO is empty

BSPI1->TXR = RDSR<

while(!(BSPI1->CSR2&BSPI_TFE)); // Wait until the Transmit FIFO is empty

while(BSPI1->CSR2&BSPI_RFNE) dummy = BSPI1->RXR; // Clear the RX Fifo.

BSPI1->TXR = 0; // dummy write to generate a read clock

while(!(BSPI1->CSR2&BSPI_RFF)); // Wait until data is received in FIFO (FIFO full)

dummy = (BSPI1->RXR) >>8; // Read the received data

Latch1_BitWrite(LATCH_CS_FR,1); // Deselect device

return dummy;

}

halim
Associate II
Posted on October 11, 2005 at 11:51

Hi,

Could you please send me if possible your hardware designe and the FRAM reference.

tj2
Associate II
Posted on October 11, 2005 at 11:59

Hi

I cannot give you the whole schematic. But we use a FM25Cl64 from Ramtron and the wiring is as this:

FM25CL64.SI -> STR710.S1.MOSI

FM25CL64.SO -> STR710.S1.MISO

FM25CL64.SCK -> STR710.S1.SCLK

FM25CL64.!CS -> Latch on EMI

FM25CL64.!Hold -> STR710.!RSTIN

FM25CL64.!WP -> STR710.!RSTIN

halim
Associate II
Posted on October 11, 2005 at 12:22

Hi,

You use GPIO0.7 in your application ?

Best regards,

Punto

tj2
Associate II
Posted on October 11, 2005 at 12:26

No. It is left unconnected and it is not initialized at any time. So I believe the pin is being pulled up by the internal pull-up (reset-state).

halim
Associate II
Posted on October 11, 2005 at 13:33

Could you please replace your function framReadStatusReg() by this function:

u8 framReadStatusReg() {

u8 dummy;

u16 TempValue;

Latch1_BitWrite(LATCH_CS_FR,0); // Select device

while(BSPI1->CSR2&BSPI_RFNE) dummy = BSPI1->RXR; // Clear the RX Fifo.

while(!(BSPI1->CSR2&BSPI_TFE)); // Wait until the Transmit FIFO is empty

BSPI1->TXR = RDSR<

while(!(BSPI1->CSR2&BSPI_TFE)); // Wait until the Transmit FIFO is empty

while(BSPI1->CSR2&BSPI_RFNE) dummy = BSPI1->RXR; // Clear the RX Fifo.

BSPI1->TXR = 0xAA; // dummy write to generate a read clock

while(!(BSPI1->CSR2&BSPI_RFF)); // Wait until data is received in FIFO (FIFO full)

TempValue = BSPI1->RXR;

dummy = (TempValue ) >>8; // Read the received data

Latch1_BitWrite(LATCH_CS_FR,1); // Deselect device

return dummy;

}

please compile, run it and check the TempValue and dummy value

tj2
Associate II
Posted on October 11, 2005 at 13:47

I've compiled and run the code. Both the TempValue and Dummy value is still 0x00.

It's strange because the correct value is shown at memory adress 0xC000B000 (BSPI1) when i make a break after the function has been executed. Somehow the receive buffer is read too early...

halim
Associate II
Posted on October 11, 2005 at 14:00

Hi

I think that we must Deselect device (!CS high) before write value from the STR7(see datasheet)

that's why i suggest to try this example:

u8 framReadStatusReg() {

u8 dummy;

u16 TempValue;

Latch1_BitWrite(LATCH_CS_FR,0); // Select device

while(BSPI1->CSR2&BSPI_RFNE) dummy = BSPI1->RXR; // Clear the RX Fifo.

while(!(BSPI1->CSR2&BSPI_TFE)); // Wait until the Transmit FIFO is empty

BSPI1->TXR = RDSR<

while(!(BSPI1->CSR2&BSPI_TFE)); // Wait until the Transmit FIFO is empty

while(BSPI1->CSR2&BSPI_RFNE) dummy = BSPI1->RXR; // Clear the RX Fifo.

BSPI1->TXR = 0xAA; // dummy write to generate a read clock

while(!(BSPI1->CSR2&BSPI_RFF)); // Wait until data is received in FIFO (FIFO full)

Latch1_BitWrite(LATCH_CS_FR,1); // Deselect device

TempValue = BSPI1->RXR;

dummy = (TempValue ) >>8; // Read the received data

return dummy;

}

tj2
Associate II
Posted on October 11, 2005 at 14:12

Tried and tested... without any luck.