2026-05-25 10:29 AM - last edited on 2026-05-25 1:19 PM by Peter BENSCH
Hello, world. I try to find answer how read that code: 2020L.
Full text on chip are:
M27C801
-100F1
52987
-2020L
SINGAPORE
That 2020L need read like: WWYXX? Or YWWXX? Thank you for answer. Regards
2026-05-25 12:43 PM
Hello @Perets and welcome the the ST community,
That product has been obsolete for years.
To answer your question and I'm not sure that's the week of the fabrication: year: 2000 week: 20.
2026-05-25 12:46 PM
I'm very sorry that I post first in wrong topic, sir. Thank you for answer! But how can be sure? Question are: if that possible that very old ST chip manufactured in 1992? Thank you for each information, sir. Regards
2026-05-25 12:50 PM
There is also a PTN 10/5894 (Product Termination Notice) from 2010, according to which all EPROMs were last delivered in 2011 - so, as @mƎALLEm said, a very, veeeery long time ago.
Regards
/Peter
2026-05-25 12:54 PM
Thank you very much, sir. Question are: chip can be from 1992 or no? And, can be that from years2020? Thank you very much :folded_hands:
2026-05-25 12:59 PM - edited 2026-05-25 1:07 PM
@Perets wrote:
But how can be sure?
No one can be sure here and EPROM devices have been depricated for a long time ago and no ST employee can give the verdict.
@Perets wrote:
Question are: if that possible that very old ST chip manufactured in 1992?
I'm deducing the age of that part number from the datasheet first release date (I'm just speculating here). First release date is september 1998. So I suppose the device was born around that date.
@Perets wrote:
can be that from years2020?
No. That doesn't make sense.
2026-05-25 1:15 PM
That very good answer, sir! Let me wait 24h (maybe somebody else can add something) and I will accept your answer like a solution. Again, thank you very much.