cancel
Showing results for 
Search instead for 
Did you mean: 

Problem during setup under Win XP sp2

andrea239955
Associate II
Posted on October 11, 2005 at 13:45

Problem during setup under Win XP sp2

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
andrea239955
Associate II
Posted on September 28, 2005 at 06:27

hi,

I'have installed the ST7 toolkit under winxp with sp2. After the software install, it ask to me that haven't found the parallel driver, and next the system crash (with blue screen) and restart! :-W

I'm not able to use the st7 software!! :-[

please help me! :o

tnx! :-]

henrik239955
Associate II
Posted on September 28, 2005 at 15:50

I had the same problem first, but then I manually removed parstm.sys from c:\windows\system32\drivers and reinstalled the tool-kit. The installation then completes without crash and the tool-kit worked ok!

/bood

andrea239955
Associate II
Posted on September 29, 2005 at 06:22

first of all thanks for your response!

i've tried this solution, but doesn't work for me.

I receive blue screen error BAD_POOL_CALLER

:-[

andrea239955
Associate II
Posted on September 29, 2005 at 08:32

I've solved the problem removing an additional Serial/Parallel card that I've installed on this machine... thanks

info45
Associate II
Posted on October 11, 2005 at 13:45

Hy,

I use WXP Home SP2 on notebook but I have'nt Your problem.

Is the parallel port used fro EMU tools?

I use EMU 3 trhouth LAN without problem!

Bye