2024-12-23 7:23 AM
Both STuW81300 and STW81200 have the option of using an external VCO but the inputs characteristics aren't specified anywhere. What is the input frequency range, input power/sensitivity in dBm or 50ohm match for single-ended input? There is one application diagram showing VCO output with a coupling capacitor followed by a balun. Can we just ac ground the other pin instead of a balun?