cancel
Showing results for 
Search instead for 
Did you mean: 

SImulation of uPSD3354DV

andya
Associate II
Posted on April 04, 2007 at 02:51

SImulation of uPSD3354DV

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
andya
Associate II
Posted on May 17, 2011 at 11:51

Hi

Has anyone managed to get simulated serial IO running in the Keil uVision simulator for the ST uPSD3354DV?

I am trying to interface HyperTerminal to my application. I have connected COM1 to COM2 on my PC (HyperTerminal on COM1). I have setup my simulated COM port and ASSIGN it to COM2 of the PC, but I do not see any output when I write data through my serial driver. The serial driver code I have works great on-target, but no joy with simulator. The PC com ports are working fine as when I open HyperTerminal in COM2 I can read/write to and fro no problems (I do close the second HT session once I am done!)

A guy on the Keil forum suggested that perhaps the uPSD3354 simulation was not complete / working properly.

Thoughts anyone?

Cheers

Andy