cancel
Showing results for 
Search instead for 
Did you mean: 

Security Bit on STR912

jflores
Associate
Posted on February 23, 2009 at 17:34

Security Bit on STR912

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jflores
Associate
Posted on May 17, 2011 at 09:57

Currently, I am having difficulty running a program on the STR912FA processor after I set the security bit using JLink.exe program provided by IAR.

Here is the procedure I use:

1) I load the program using the IAR Embedded Workbench IDE, and start it running. This is a simple ''LED'' scan program.

2) I then stop debugging, which allows the program to continue running without the debug session.

3) I then run the program JLINK.exe, which halts the program and allows me to set the security bit using the ''secure'' command.

4) I then quit JLINK.exe

5) At that point, the program is locked up. I can see that that reset line goes low and then high when I press the reset button, but the program appears to be locked up.

Any idea why I am unable to run a program with the STR912 Security Bit set? I must be forgetting something.

Thanks

JAF

I would appreciate any help you might provide: