2008-04-14 01:30 AM
SCU_CLKCNTR - invalid values for STR91xFA?
2011-05-17 12:52 AM
Hello,
Could you please let me know if the register SCU_CLKCNTR can be configured to have an invalid value when the MCU is driven by a PLL (i.e. MCLKSEL = PLL)?2011-05-17 12:52 AM
No.
2011-05-17 12:52 AM
hello eris,
do you mean that it cannot be configured invalid or that you cannot tell me (maybe because of the same reason...)? One more thing: If I have an older revision of the chip (STR91xF revision B or D), then the only limitation is the speed of the flash (not faster than 48 MHz)? Thanks in advance