2006-03-15 09:34 PM
RVDK RVICE/ME Crash - Blue Screen of Death
2006-03-14 11:49 PM
I have 2 computers running XP PRO SP2. They were solid until installing and operating ST RVDK.
Now some times (more than enough to be annoying) simply powering off my target system will give me the fateful BLUE SCREEN OF DEATH. If any one has a fix, cluse or source for updates, it would be much appreciated.2006-03-15 09:34 PM
I have it on two different computers and several times each.
As for printing the Blue Screen of Death as it is known this is not possible. The only thing that works at this point is the reset button. It does report on the next boot up that it was a driver problem. I may take more notes next time it occurs. Donald.