cancel
Showing results for 
Search instead for 
Did you mean: 

regarding secondary flash as code space

babidesai123
Associate II
Posted on May 08, 2003 at 05:19

regarding secondary flash as code space

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
babidesai123
Associate II
Posted on May 17, 2011 at 11:53

Hello,

Can anyone tell me,for general IAP design why it is recomended that

secondary flash should contain the IAP code & primary as main application code??

Apart from the large memory area what is the major difference between the two.

If assume that application cdoe is small enough to fit into the 1 sector of secondary flash , then it is advisible to use secondary as application code area & primary as IAP code or no....

PLZ clarify
joseph2399
Associate II
Posted on May 17, 2011 at 11:53

Secondary Flash has higher priority than the Primary Flash (see Figure 51, data sheet), other than that, they should be the same. If the VM register is setup properly, IAP can reside in the Main Flash at power up also.

babidesai123
Associate II
Posted on May 17, 2011 at 11:53

Thanks alot..

purvi