2004-01-09 05:52 AM
reading the falsh content using JTAG
2011-05-17 02:53 AM
Hi,
Can we read the flash memory (full or sector) using the JTAG programming??provided that flash sector is not protected. if yes the what are the steps?? Can u give detail steps to read the flash mem content using JTAG? [ This message was edited by: Purvi on 11-04-2003 08:54 ]2011-05-17 02:53 AM
I am trying to do the same thing, and I receive the same response. Did you resolve this problem ?
2011-05-17 02:53 AM
In the PSDsoft Express there si a fuction: STMicroelectronics Conventional Programmers.
Run it, you should come into a dialog. In the dialog you press the button --- Upload. the data in the uPSD can been load. If the data is protected, you can't do it.2011-05-17 02:53 AM
just now i tried with that ..but it's showing the dialog box showing
''device upsd3234A is currently not supported under psd pro'' plz help2011-05-17 02:53 AM
If using the Flashlink do an upload in the JTAG/ISP section
Regards sjo2011-05-17 02:53 AM
Ok, but in this section I can't read the device, can I?
2011-05-17 02:53 AM
Yes, you can... in the ''Step 2'' section, the first box normal has ''Program/Verify'' selected or something of the like. Just change it to upload.