cancel
Showing results for 
Search instead for 
Did you mean: 

PWM beginners help

b_buerke
Associate II
Posted on January 10, 2005 at 10:11

PWM beginners help

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
b_buerke
Associate II
Posted on January 10, 2005 at 10:11

Hello Everybody i am new here at the forum and also new to the Microthing so maybe its a stupid message...

I need to set up my ST7FLITE29 to work with PWM Output on 250Khz and a Duty Cycle of 50%. But i cant figure out how to initialise it to do so. I dont understand the Datasheet.

I read some threads here but didnt figure out either.

I calculated the frequency to be ATR value 4080/ 0xFF0

But how do i set the DCR to get 50% and why do i have DRCH and DRCL ????

I am very confused but maybe thats normal at the beginning!

I hope there is someone who can explain whats this about and how to get to the 50%

Below is my code to initialise.

Is it right with the calculation of 4080for 250KHz?? I am running with the internal RC and 8X PLL

//initialising I/O ports

PADR = 0x1C; //setting up dataregister//

PADDR = 0x9F; //setting up datadirection//

PAOR = 0xDF; //setting up dataoptions//

PBDR = 0xFF; //Setting port B dataregisters//

PBDDR = 0x00; //Setting port B Datadirection to input//

PBOR = 0x00; //Setting port B to be floating//

/*******************************************

setting up 12-bit timer for PWM output

***********************************************/

PWMCR = 0x15; //Enabling PWM Output on PWM0, PWM1, PWM2//

ATRH = 0x0F; //Autoreloadtimer High//

ATRL = 0xF0; //Autoreloadtimer Low//

ATCSR |= 0x18; //Set Counter Clk = fCPU//

Thank a lot

Björn