cancel
Showing results for 
Search instead for 
Did you mean: 

VGA-LCD

lucio
Associate
Posted on January 11, 2005 at 19:49

VGA-LCD

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
lucio
Associate
Posted on May 11, 2004 at 11:10

Hi,

I'm using an STPC Consumer with a TFT 1024x768 LCD connected

to the on board VGA. I'm using the VGA BIOS from Elpin System.

The problem was that work at a frequency of 63Hz instead a

frequency of 60Hz. I'm not familiar with the VGA register, can you

help me to focus on the register intrested on frequency adjust

and screen centering

thanks
uwe
Associate II
Posted on January 11, 2005 at 19:49

Do you have a VGA register set example for a 1024x768 display ?

Perhaps in a 32kBios, even with 63 Hz.

Best Regards

Flipflop