cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Beginner, need help with X-Cube-ai project

jzzunn
Associate II

I need help with a project. I need to deploy a sound detection AI model to my B-U585I-IOT02A board. I want to test the model using live audio playback, im using Mimii valve dataset to train the AI. Im planning to play back the audio and test inference and see if the AI detects anomalous or normal sounds. I have trained the AI and compressed it to tflite file. But i have no idea how to use STM32. It is so confusing Im using AI chatbot to help me but i cant do it. I think i need to configure USART, MDF (for microphone) and x-cube-ai. but i dont know how to do it. Need help please.

1 REPLY 1
Julian E.
ST Employee

Hello @jzzunn ,

 

I highly recommend using ST Model ZOO: 

STMicroelectronics/stm32ai-modelzoo-services: AI Model Zoo services for STM32 devices

 

In you case you want to use the Audio event detection use case and the deployment operation mode:

stm32ai-modelzoo-services/audio_event_detection/deployment/README.md at main · STMicroelectronics/stm32ai-modelzoo-services

 

Just to give you some context:

ST Model Zoo is a repository to help you train, quantize, benchmark and deploy AI to STM32 Microcontrollers.

The way it work is that you bring your own model (or one from our repository) and your data and you use the user_config.yaml file to define what you want to do:

  • Model path
  • Data path
  • Operation mode (training, benchmark, deployment etc)
  • Other parameters specific to each operation modes

Then you run the python script stm32ai_main.py to do what you've defined.

 

ST Model Zoo is splitted in 2 github repository: ST Model Zoo and ST Model Zoo services. 

One contains models that you can use, the other the python scripts.

 

The deployment operation mode allows you to flash a complete demo firmware with your model.

You can find the firmware source files as a STM32CubeIDE project in the folder /application_code

 

To install ST Model Zoo services, make sure to follow the before you start:

stm32ai-modelzoo-services/audio_event_detection/deployment/README.md at main · STMicroelectronics/stm32ai-modelzoo-services

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.