Skip to main content
digisys99
Associate
October 29, 2008
Question

Psdsoft programming tip required!

  • October 29, 2008
  • 1 reply
  • 625 views
Posted on October 29, 2008 at 17:56

Psdsoft programming tip required!

This topic has been closed for replies.

1 reply

digisys99
digisys99Author
Associate
May 17, 2011
Posted on May 17, 2011 at 11:52

I mapped to use big flash(128K) for data and small one (32K) for code.

As sector is only 8K in secondary flash, how I could declare using PSDsoft?

As my program is bigger than 8K, do I have to declare same hex file for all for sectors in Merging MCU pane???

Thank's!

Here final report...

Memory Start Stop Memory

Block Address Address Data File

--------------------------------------------------------------------------

FS0 [00000 - 07FFF]

FS1 [08000 - 0FFFF]

FS2 [10000 - 17FFF]

FS3 [18000 - 1FFFF]

FS4 [20000 - 27FFF]

FS5 [28000 - 2FFFF]

FS6 [30000 - 37FFF]

FS7 [38000 - 3FFFF]

CSBOOT0[40000 - 41FFF] 0000 1FFF test.hex

CSBOOT1[42000 - 43FFF]

CSBOOT2[44000 - 45FFF]

CSBOOT3[46000 - 47FFF]