2005-05-17 11:36 PM
2005-05-09 03:51 AM
dear sjo,
I have made flashbash and successful to program st72c334n4. now i use it to program st7flite09 and found some problem. programmer serial port test is ok, I can write optionbyte, but I can not write the flash erea. an error message is displayed ''operation Failed'' , coudl you help me solve this problem. best regards,2005-05-17 11:36 PM
If option bytes are being programmed successfully, it indicates successful communication and proper Flash function/ICC. But, did you check the Flash memory mapping in the 334 you are using and the Lite09?