2005-12-19 9:31 PM
Problems with ST7MDT2-EMU2B and ST7 visual develop. SW
2005-12-19 2:23 AM
Hi.
I have 2 problems. 1. I have a ST7MDT2-EMU2B emulator and I would like to have this emulator to work on windows XP. I can't connect to the device? I'm aware that the datasheet says that I should run the device on a 95/98/NT machine. Has ST made a LPT driver for 2000/XP? 2. I have a SW that has been written in CodeWarrior IDE, and I would like to have this code running in the ST7 visual develop. 3.00 SW. I choose the ''Metrowerks'' under ''Linker'' and then I add the *.c and *.h files to the project. When I compile / build the project, it comes up with all kinds of errors... The code can be compiled under the CodeWarrior IDE with NO errors at all. How can I make the ST7 visual develop. SW compile the code the right way and get to working with the debugger (ST7MDT2-EMU2B)? What am I doing wrong? Thanks in advance. Regards. Peter Denmark2005-12-19 9:31 PM
Hi,
1. You should have an old datasheet, because the EMU2B works now with XP and W2000 2. Did you select MW when you create your workspace in the toolchain text box ? Did you select your PRM or keep the default one ? ''All kind of errors'' is not very helpful to help you. If you can give us more clues! BR laurent [ This message was edited by: laubey on 20-12-2005 15:16 ]