Posted on May 17, 2011 at 11:52I bought the RLINK.
I have some problem program my PSD834F2.
I have in the same board one MAX7000S of Altera and one PSD834F2 of PSD - ST Microelectronics. They share the same 4-wire JTAG port ( TDI,TDO,TCK,TMS).
With the PSDsoft the Rlink Connect Test was Ok, the Target Connect Test was ok. But I have this error when I try to program PSD:
PSD JTAG-ISP Operations
PSDsoft Express 8.61 Copyright (C) 1993-2005 STMicroelectronics, Inc. All Rights Reserved.
DATE : 04/27/2009 TIME : 18:56:59
Device 1 : ( 4 pins )
ERROR: Communication (0303)
Hint: Unable to read device ID for checking.
Please check that the device is correctly connected through the JTAG port.
Time elapsed : 1 sec.
I have my Altera in ByPass...
What am I doing wrong?
I have the latest version of PSDsoft. Do I have to update the software RLINK? Jungo 01/04/2004 6.2.0.0.
Help Please.