2003-05-27 4:41 AM
2003-05-27 2:52 AM
Hello,
I test my new kernel with: 1.General Software BIOS+LILO 2.Phoenix BIOS+LILO This is the same kernel I used with stpc loader. I have the following result: 1.with the General Software BIOS after I chose the operating system from the LILO menu the system restart automatically. In the lilo.conf file I added vga=ask (and install the new loader by running the lilo command in the terminal window) but it has the same affect. 2.With the Phoenix BIOS the system is also restart automatically but when I added vga=ask in the lilo.conf file and restart the computer I chose the new resolution and the linux didn’t continue to load. It beeps 8 times and the POST code show 22. I attach the new kernel I created. What do you advice me to do? Thanks in advance.2003-05-27 4:41 AM
With a solution BIOS+LILO, you must use the bzImage version of the kernel you get in usr/src/linux/arch/i386/boot after a 'make bzImage'. It is not exactly the same as the vmlinux you get from usr/src/linux.
Even if the frame buffer device is not well installed, your kernel should work at least in text mode. Farfalla