2025-03-04 7:35 AM
Hello everyone
I'm working on a student project with an STM35H563RIT6 and a Power over Ethernet (PoE) supply. I'm currently validating my design, but, reading the datasheet of the PM8805TR to do PoE, I just see the output current (max 2A) but no voltage (except VOB everywhere in the datasheet without any really data on it).
Did I passed over it without seeing the information ? Or are there any calculation to identify the output voltage ?
Thanks in advance for your answer
Kind regards
Sappherien