2019-06-26 4:35 PM
Hello,
I have the STM32F446RE board and would like to try out WiFi programming. I have been looking at ESP8266 but can't find a lot written about STM32 Discovery boards interfacing with the module. I understand that this module is communicated with through the UART and the AT command set. But I am concerned because all mention of the ESP8266 discuss the problem of the voltage (3.3V vs 5V). Is there any good tutorial on setting up a dev system for doing wi-fi programming.
Thank you,
Michael Uman