2005-03-10 3:42 AM
2005-03-10 2:39 AM
Hi Everybody
Is anyone know of PC SPI protocol. I need this in order to down load my final firmware (I dont have debug port in the final design). Thanks HKobi2005-03-10 3:42 AM
Perhaps I am wrong, but I am not aware of a PC SPI protocol.
SPI stands for Serial Periferal Interface. The communication takes place between a master and a slave. Both of them use a shift register that is updated by means of three wires: MISO (master in - slave out), MOSI (master out - slave in) and SCK (serial clock). The data transmission is byte-oriented, but there is no protocol that states the meaning of the exchanged data. To talk to a PC, it is better to use a microcontroller with a SCI (Serial Communication Interface). In this case you have to use a MAX232 to make the signal compatible with RS232 (aka COM ports of a PC). It is more difficult to interconnect a PC with SPI, since you have to build custom hardware and attach it to a parallel port. Even if you have a communication mean with the PC, it is up to you to implement the In Application Programming. I suggest you to read the datasheet of the microcontroller that you are using, the ''Flash Programming Reference Manual'', AN1576 and AN1576. Regards EtaPhi