Skip to main content
js3
Associate
May 29, 2004
Question

pb with Flash Link

  • May 29, 2004
  • 2 replies
  • 807 views
Posted on May 29, 2004 at 03:25

pb with Flash Link

This topic has been closed for replies.

2 replies

js3
js3Author
Associate
May 17, 2011
Posted on May 17, 2011 at 12:01

iwant to program the flash memory of my µPSD3254A with FlashLink

so I've installed PSDsoft Express (8.10) on my computer. But after this installation I've discovered that there is a problem with the window NT parallal port driver to enable JTAG process (jtag driver is not installed or not started).

consequence :

after my computer reboot, the os don't run normally(systeme crash).

now ican restart it because I've uninstalled the sofware.

So , Have you a solution to debug my situation??

I've got an IBM ThinkCenter computer with an intel pentium4 and windows XP Professionnal (SP1).

joseph2399
Associate II
May 17, 2011
Posted on May 17, 2011 at 12:01

Please see FAQ #109 at:

http://www.st.com/stonline/products/families/memories/psm/psdfaq.htm