cancel
Showing results for 
Search instead for 
Did you mean: 

openOCD security bit

udo1
Associate
Posted on July 08, 2008 at 10:40

openOCD security bit

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
udo1
Associate
Posted on May 17, 2011 at 09:54

Hello,

I'm trying to set the security-bit on a STR912FAW44. I found a PDF (http://www.st.com/stonline/products/literature/pm/11659.pdf) that describes which register needs to be set but I have no idea how to do this using openOCD. I use a wiggler-compliant jtag device to program the processor.

sjo
Associate II
Posted on May 17, 2011 at 09:54

the security bit is the using the str9xpec driver

so in your config you need the str9xpec driver:

flash bank str9x 0x00000000 0x00080000 0 0 0

flash bank str9x 0x00080000 0x00008000 0 0 0

flash bank str9xpec 0x00000000 0x00080000 0 0 0

# assert reset (srst)

#jtag_reset 0 1

then to lock the device

# enable turbo mode

str9xpec enable_turbo 2

# lock str9

str9xpec lock 2

# disable turbo

str9xpec disable_turbo 2

# let device run - resetting tap aswell

jtag_reset 1 1

jtag_reset 0 0

see the following for more info:

http://forum.sparkfun.com/viewtopic.php?t=9451

Cheers

sjo

[ This message was edited by: sjo on 08-07-2008 14:11 ]