cancel
Showing results for 
Search instead for 
Did you mean: 

Newbie to STR7 - timers frequency calculation

michael
Associate II
Posted on March 27, 2008 at 06:23

Newbie to STR7 - timers frequency calculation

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
michael
Associate II
Posted on March 27, 2008 at 06:07

Hello,

I am new to the STR7 and I was hoping you'd be able to clarify something simple for me: I have configured my processor with the following code:

Code:

<BR> RCCU_MCLKConfig(RCCU_DEFAULT); // MCLK = RCLK <BR> RCCU_FCLKConfig(RCCU_RCLK_2); // FCLK = RCLK/2 <BR> RCCU_PCLKConfig(RCCU_RCLK_4); // PCLK = RCLK/4 <BR> RCCU_PLL1Config(RCCU_PLL1_Mul_12, RCCU_Div_2); // 48MHz PLL @ 16MHz XTAL <BR>

Now I have read the data sheet, but I don't understand how the period of my TIM3 is calculated to be ~10[ms] with the prescaler 1, when it is fed by PCLK2 (whose speed is 12 MHz). I also don't understand why CNTR input frequency is 6000 kHz. Could you please clarify HOW the 12 MHz input clock ends up as a 10[ms] period of TIM3? I calculated all these numbers with STR71x_Calculation.xls.

Thanks in advance!

[ This message was edited by: michael.tamir on 27-03-2008 10:38 ]

michael
Associate II
Posted on March 27, 2008 at 06:23

I figured it out myself, thanks anyway.