2026-04-24 6:28 PM
Hello,
I am using a STM32WL55 UFQFPN48 in an application. I am only using the high power output (up to +22 dBm) and only plan on transmitting with this device.
I want to transmit in the 420-440 MHz range, but there does not seem to be any load-pull analysis data from within AN5457 which would give output impedance at this frequency. I can only find data for higher bands.
Is this data found somewhere else? I would like to use it for simulation and calculation.
Best
Solved! Go to Solution.
2026-04-27 12:00 AM
Hello,
I can provide the optimum load for 490 MHz at 22 dBm.
Zopt = 14+ j10
P_level (dBm) = 22 dBm
Pout = 21.9 dBm
IBAT = 108.5 mA
Best regards
Saverio
2026-04-27 12:00 AM
Hello,
I can provide the optimum load for 490 MHz at 22 dBm.
Zopt = 14+ j10
P_level (dBm) = 22 dBm
Pout = 21.9 dBm
IBAT = 108.5 mA
Best regards
Saverio