cancel
Showing results for 
Search instead for 
Did you mean: 

Need code sample for timer interrupts.

jonny_bee_henry
Associate II
Posted on October 19, 2006 at 07:37

Need code sample for timer interrupts.

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
jonny_bee_henry
Associate II
Posted on May 17, 2011 at 09:33

I cannot figure out how to get a timer to generate an interrupt at a fixed interval. This question has been asked here at least twice recently, and both times was answered with an incomplete code fragment that I cannot compile (using the IAR dev kit). For example, I just want to configure TIM0 to interrupt every 10ms, and have its interrupt service routine increment a global counter that I can print out periodically in the main loop. Can someone please provide the code to do that?

egads
Associate II
Posted on May 17, 2011 at 09:33

Keil's STR9 ''Blinky'' example has a timer based interrupt example.

I think you can down load this from the keil website. I know thi sis not an IAR example, but maybe it will lead you down the correct path!

jonny_bee_henry
Associate II
Posted on May 17, 2011 at 09:33

Thanks for the pointer, but I'm looking for sample code using the STR91x library functions so that I can understand how they work (i.e what I'm doing wrong). The Keil example doesn't use the library.

jonny_bee_henry
Associate II
Posted on May 17, 2011 at 09:33

Maybe if I just give my code, somebody can find the problem:

main.c

------

#include ''91x_lib.h''

#include

int IRQ_counter = 0;

main() {

TIM_InitTypeDef TIM0_InitStructure;

// usual clock & uart initialization, etc. omitted

/* TIM0 Initialization */

#define TIM0Prescaler 0xFF

#define PWMFreqInHz 100

#define PWMPulsePercent 33

SCU_APBPeriphClockConfig(__TIM01, ENABLE);

TIM_DeInit(TIM0);

TIM_StructInit(&TIM0_InitStructure);

/* TIM0 Configuration in PWM Mode */

TIM0_InitStructure.TIM_Mode = TIM_PWM;

TIM0_InitStructure.TIM_Clock_Source = TIM_CLK_APB;

TIM0_InitStructure.TIM_Prescaler = TIM0Prescaler;

TIM0_InitStructure.TIM_Pulse_Level_1 = TIM_HIGH;

TIM0_InitStructure.TIM_Period_Level = TIM_LOW;

TIM0_InitStructure.TIM_Full_Period = (SCU_GetMCLKFreqValue())*1000 / ((TIM0Prescaler + 1) * PWMFreqInHz);

TIM0_InitStructure.TIM_Pulse_Length_1 = TIM0_InitStructure.TIM_Full_Period * PWMPulsePercent / 100;

TIM_Init (TIM0, &TIM0_InitStructure);

/* Enable and configure the priority of the IRQ Channel*/

SCU_AHBPeriphClockConfig(__VIC, ENABLE);

VIC_DeInit();

VIC_Config(TIM0_ITLine, VIC_IRQ, 0);

VIC_ITCmd(TIM0_ITLine, ENABLE);

TIM_ITConfig(TIM0, TIM_IT_TO, ENABLE);

TIM_CounterCmd(TIM0, TIM_START);

while (1) {

if (IRQ_counter % 100 == 0)

putchar('.');

}

}

91x_it.c

---------

void TIM0_IRQHandler(void)

{

extern int IRQ_counter;

IRQ_counter++;

TIM_ClearFlag(TIM0, TIM_FLAG_TO);

}

Posted on May 17, 2011 at 09:33

hi jonny_h

I use a similar configuration but with a

different irq event:

/* Enable the Timer Overflow interrupt */

TIM_ITConfig(TIM0, TIM_IT_OC2, ENABLE);

I'm not sure but for what I understand the

pwm mode doesn't trig the Timer overflow (TO).

If you like to use the TO event I suggest to you to

use a different configuration for the timer, like

output compare mode

egads
Associate II
Posted on May 17, 2011 at 09:33

Quote:

On 18-10-2006 at 00:34, Anonymous wrote:

The Keil example doesn't use the library.

To me that's a positive. I find the ST lib stuff to be overly complicated and written in a way that is hard to figure out what its doing. I'm much more comfortable configuring my peripherals with simple writes to registers.

yuantuh
Associate II
Posted on May 17, 2011 at 09:33

hi jonny_h,

Are you all right? Try the following piece of code please. It works in my board.

#include ''91x_lib.h''

#define TIM0Prescaler 0xFF

#define PWMFreqInHz 100

#define PWMPulsePercent 33

TIM_InitTypeDef TIM_InitStructure;

void TIM0_IRQHandlerInvoked(void)

{

// balah balah

// ...

/*Clear the TIM_TO flag for the next interrupt*/

TIM_ClearFlag(TIM0, TIM_FLAG_TO);

}

void main(void)

{

#ifdef DEBUG

debug();

#endif

/*-------------------- System Clock Config --------------------*/

SCU_MCLKSourceConfig(SCU_MCLK_OSC);

// Someone said PLL = 96 MHz is unstable, so change PLL = 48 MHz

//SCU_PLLFactorsConfig(0xC0, 0x19, 0x2); // PLL = 96 MHz

SCU_PLLFactorsConfig(0xC0, 0x19, 0x3); // PLL = 48 MHz

SCU_PLLCmd(ENABLE);

SCU_MCLKSourceConfig(SCU_MCLK_PLL);

/* Enable VIC clock */

SCU_AHBPeriphClockConfig(__VIC,ENABLE);

VIC_DeInit();

/* Enable TIM0 clock */

SCU_APBPeriphClockConfig(__TIM01, ENABLE);

TIM_DeInit(TIM0);

TIM_StructInit(&TIM_InitStructure);

TIM_InitStructure.TIM_Mode = TIM_PWM;

TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB;

TIM_InitStructure.TIM_Prescaler = 0xFF;

TIM_InitStructure.TIM_Pulse_Level_1 = TIM_HIGH;

TIM_InitStructure.TIM_Period_Level = TIM_LOW;

TIM_InitStructure.TIM_Full_Period = (SCU_GetMCLKFreqValue())*1000 / ((TIM0Prescaler + 1) * PWMFreqInHz);

TIM_InitStructure.TIM_Pulse_Length_1 = TIM_InitStructure.TIM_Full_Period * PWMPulsePercent / 100;

/* Initialize the Timer 0 */

TIM_Init (TIM0, &TIM_InitStructure);

/* Enable the Timer Overflow interrupt */

TIM_ITConfig(TIM0, TIM_IT_TO, ENABLE);

VIC_Config(TIM0_ITLine, VIC_IRQ, 4);

VIC_ITCmd(TIM0_ITLine, ENABLE);

/* Start the Timer counter */

TIM_CounterCmd(TIM0, TIM_START);

while(1)

{

// balah balah

// ...

}

}

in 91x_it.c

---------

extern void TIM0_IRQHandlerInvoked(void);

void TIM0_IRQHandler(void)

{

TIM0_IRQHandlerInvoked();

}

91x_it.h

#ifndef __91x_CONF_H

#define __91x_CONF_H

#define DEBUG

#define _VIC

#define _VIC0

#define _TIM

#define _TIM0

#define _SCU

#ifndef _Main_Crystal

#define _Main_Crystal 25000

#endif

#endif

craig239955_st
Associate II
Posted on May 17, 2011 at 09:33

I use following code on my KEIL STR9 evaluation board.

Timer 1 is used as a 1mS interrupt generator, 2 others are used a counters.

Luc Vercruysse.

Robosoft n.v.

__irq void TIM1_IRQHandler (void)

{

test = test + 1;

TIM_ClearFlag(TIM1,TIM_FLAG_OC1); //Clear pending interrupt flag

VIC0->VAR = 0x0000; //End of interrupt

VIC1->VAR = 0x0000;

TIM1->OC1R += 200; //every 1mS

}

extern __irq void TIM1_IRQHandler(void);

extern long test;

TIM_InitTypeDef Timer ;

GPIO_InitTypeDef GPIO;

int main (void) {

//Interrupt setup

SCU_APBPeriphClockConfig(__VIC,ENABLE);

VIC_DeInit();

VIC_Config(TIM1_ITLine,VIC_IRQ,1);

VIC_ITCmd(TIM1_ITLine,ENABLE);

//Timer Setup

SCU_APBPeriphClockConfig(__TIM01, ENABLE); /* Enable the clock for TIM0 and TIM1 */

SCU_APBPeriphClockConfig(__TIM23, ENABLE); /* Enable the clock for TIM0 and TIM1 */

TIM_DeInit(TIM0); /* TIM0 Deinitialization */

TIM_DeInit(TIM1); /* TIM1 Deinitialization */

TIM_DeInit(TIM2); /* TIM2 Deinitialization */

SCU_TIMCLKSourceConfig(SCU_TIM01,SCU_TIMCLK_EXT);

SCU_TIMCLKSourceConfig(SCU_TIM23,SCU_TIMCLK_EXT);

//Init Counter 0 (as a counter)

Timer.TIM_Mode = TIM_OCM_CHANNEL_1;

Timer.TIM_Clock_Source = TIM_CLK_EXTERNAL;

Timer.TIM_Clock_Edge = TIM_CLK_EDGE_RISING;

TIM_Init (TIM0, &Timer);

TIM_CounterCmd(TIM0,TIM_CLEAR);

TIM_CounterCmd(TIM0,TIM_START);

//Init Counter 2 (as a counter)

Timer.TIM_Mode = TIM_OCM_CHANNEL_1;

Timer.TIM_Clock_Source = TIM_CLK_EXTERNAL;

Timer.TIM_Clock_Edge = TIM_CLK_EDGE_RISING;

TIM_Init (TIM2, &Timer);

TIM_CounterCmd(TIM2,TIM_CLEAR);

TIM_CounterCmd(TIM2,TIM_START);

//Init Timer 1 (1 mSinterrupt (FCLK = 96MHz)

Timer.TIM_Mode = TIM_OCM_CHANNEL_1;

Timer.TIM_Clock_Source = TIM_CLK_APB;

Timer.TIM_Clock_Edge = TIM_CLK_EDGE_RISING;

TIM_Init (TIM1, &Timer);

TIM_PrescalerConfig(TIM1,240);

TIM_CounterCmd(TIM1,TIM_START);

TIM_ITConfig(TIM1,TIM_IT_OC1,ENABLE); //output capture

.....

}