2004-03-15 7:39 PM
Need a lil helping hand on accessing the EEPROM on a ST6260
2004-03-15 1:50 AM
Hier a lil routine that works propper on the Epromversion
of the ST6260B. The same routine does not work on the OTA version of the 6260C. Please, I am happy for any hint. setAD LDI DWDR,0FFh ; JRS E2BUSY,EECTL,setAD ; LDI EECTL,00h ; doAD LDI DWDR,0FFh ; JRS E2BUSY,EECTL,doAD ; LDI DRBR,00000001b ; LD A,SData ; ANDI A,00001111b ; SET E2ENA,EECTL ; doAD1 LDI DWDR,0FFh ; JRS E2BUSY,EECTL,doAD1 ; LD EEDat,A ; goonAD LDI DWDR,0FFh ; JRS E2BUSY,EECTL,goonAD ; RES E2ENA,EECTL ; getAD LDI DWDR,0FFh ; JRS E2BUSY,EECTL,getAD ; LDI DRBR,00000001b ; LDI EECTL,00h ; getAD0 LDI DWDR,0FFh ; JRS E2BUSY,EECTL,getAD0 ; LD A,EEDat ; ANDI A,00001111b ; LD EAdress,A ; SET E2off,EECTL ; RET ; Note: EEDat = 10h greetinx Joker[ This message was edited by: JRN-Joker on 15-03-2004 15:23 ]2004-03-15 7:39 PM
hi, sorry for bad english
not use set o res in to route for read or write e2prom, but use only LDI eectl,xx This route work very well on the ST62E65C, first use this route disable all interrupts rde2p ld a,e2p_id ;adress e2prom ld x,a ldi xcount,8 ldi y,dato0 ;adress ram when save the buytes read ldi drbr,01h ;Select the EEPROM page 0 ldi eectl,00h ;Enable the EEPROM rde2p1 ldi wdr,0ffh jrs 1,eectl,$ ld a,(x) ld (y),a inc x inc y dec xcount jrnz rde2p1 ldi wdr,0ffh ldi eectl,40h ;Disable the EEPROM (Low comsuption) ret wre2p ld a,e2p_id ;adress e2prom ld x,a ;adress -> X ldi xcount,8 ;number byte to save ldi y,dato0 ;adress ram byte to save ldi drbr,01h ;Select the EEPROM page 0 ldi eectl,05h ;Enable EEPROM parallel writing mode ldi wdr,0ffh jrs 1,eectl,$ ;check that e2pron not busy wre2p1 ld a,(y) ld (x),a inc x inc y dec xcount ;decrement counter jrz wre2p2 jp wre2p1 wre2p2 ldi wdr,0ffh ldi eectl,0dh ;Start parallel writing (5ms typical) jrs 1,eectl,$ ;wait end procedure ldi eectl,40h ;Disable the EEPROM (Low comsuption) ldi wdr,0ffh ret