cancel
Showing results for 
Search instead for 
Did you mean: 

MIPI_DSI ESD protection

DonPotokon
Associate II

DonPotokon_0-1738929627492.png

Hello, this is the ECMF4-40A100N10(MIPI DSI ESD protection). I want to implement it in my design and I was wondering if it matters to connect your positive differential pair signals to D1+ and D2+ and negative to D-. Or can  acually flip them? So I connect my negative differential pair signals to D+ and positive to D-. That way I can route it much easier. Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

OK, now it's clear: yes, you can do that, because the differential pairs are symmetrical in themselves..

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Somehow your idea is still unclear to me:

It does not matter which differential pair you connect to which (paired) port. You must therefore connect one differential line pair to D1+, D1- and the other to D2+, D2-.
But you can't connect one differential line pair to D1+, D2+ and the other to D1-, D2-, because then the common mode filters can no longer do their job.

Does that answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

DonPotokon_0-1738937391759.png

I am sorry, I maybe overcomplicated it a bit...So my only concern is whether I can route MIPI CLK_P  to D2- and CLK_N to D2+. And the same way on data line. I think there is no problem with that but just to be 100% sure.

Thanks for the reply and Best Regards

JP

Peter BENSCH
ST Employee

OK, now it's clear: yes, you can do that, because the differential pairs are symmetrical in themselves..

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.