cancel
Showing results for 
Search instead for 
Did you mean: 

May I exchange the in/out of EMIF03-SIM02M8?

diverger
Senior

Hi,

May I exchange the in/exit of the EMIF03? As the pin name indicate there are in pins and exit pins. But from the internal diagram, the ins and outs are exchangeable.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
FGUIT
ST Employee

Hi,

Unfortunately, IN and OUT cannot be exchanged, as external pins withstand +/-8kV ESD contact discharge, +/-15kV ESD air discharge, whereas internal pins withstand +/-2kV ESD contact and air discharge. So, external pins are compliant with IEC 61000-4-2 level 4, which is not the case for internal pins. External pins need to be connected to SIM socket, internal pins to SIM card reader IC. However, RST and DATA can be exchanged, as schematic is the same.

Best regards.

Fabrice. 

View solution in original post

1 REPLY 1
FGUIT
ST Employee

Hi,

Unfortunately, IN and OUT cannot be exchanged, as external pins withstand +/-8kV ESD contact discharge, +/-15kV ESD air discharge, whereas internal pins withstand +/-2kV ESD contact and air discharge. So, external pins are compliant with IEC 61000-4-2 level 4, which is not the case for internal pins. External pins need to be connected to SIM socket, internal pins to SIM card reader IC. However, RST and DATA can be exchanged, as schematic is the same.

Best regards.

Fabrice.