2007-05-15 01:39 AM
2011-05-17 12:43 AM
I use Keil mVISION3.
What is the Image Entry Point writen in map file: Memory Map of the image Image Entry point : 0x0008023c Load Region LR_IROM1 (Base: 0x00080000, Siz................... ................................................................ Is the Image Entry point is the address to jump after Flash writing? If it so where this value(0x0008023c(not same for different aplications)) located in address range? [ This message was edited by: kesart on 16-05-2007 08:25 ]