2019-05-27 7:11 AM
Hello,
When i am trying read/write operation on M95M01 by connecting my board to JTAG supply, my m95M01 EEPROM is working correctly as i can debug it and see.
But when i am supplying my M95M01 EEPROM through an adapter it reads 0xFF. What can be the issue?
Do i need to do any initialization?
Also its getting enough voltage of 3.3V as i can measure through multimeter.
Thank you,
Akshay
2019-06-04 9:38 AM
Hello,
No need initialization.
Usually when read data = 0xFF (and memory content supposed to be different) means that the device is not selected.
3V3 is good. Check your frequency : max 10MHz
BR
ST EEPROM team suPPort