2004-04-29 5:47 AM
2011-05-17 3:00 AM
I am trying to develop a jtag device for uPSD3233B.
Now,i success read the IDCODE of the target mcu, but i have no idea of knowing the security status. Can anybody tell me how to do this?Supplying sample code would be advantage. Regards.2011-05-17 3:00 AM
As we know,IEEE11 descript the JTAG port.
I am using the standard mode,4 pin were used(TDI,TDO,TMS,TCK) by MCS- Pls tell me how to reprogram and erase the target mcu. I also want to know that,where can i download some documents about designing software for JTAG. Thanks.2011-05-17 3:00 AM
STMicroelectronics offers PSDsoft (Windows application) in conjuction with FlashLink (JTAG dongle) for programming the uPSD products via JTAG. You can download PSDsoft from the following webpage:
http://www.st.com/stonline/products/families/memories/psm/soft_c2.htm
For more information on FlashLink, go to the following webpage:2011-05-17 3:00 AM
Thanks.
I have another question,when i perform ISC-SPECIAL,there are for commands as the following list: ISC-SPECIAL(ERASE) ISC-SPECIAL(PGM) ISC-SPECIAL(NONE) ISC-SPECIAL(ERASE&PGM) There are two bits can be transfered by TDI,how can i part the value of the two bits?