2004-04-27 6:55 PM
How to do memory paging in uPSD3254BV-24U6?
2011-05-17 3:00 AM
Hi All,
Can somebody please let me know how to do memory paging that is greater than 64K in uPSD3254BV? We are using Keil to do the fireware. Here is what we set in PSDsoft: PGM SRACE: ---------- csboot0: 0000-1FFF csboot1: 2000-3FFF csboot2: 4000-5FFF csboot3: 6000-7FFF DATA SPACE: ----------- CSIOP: 0000-00FF rs0: 0100-7FFF fs0: 8000-FFFF fs1: 8000-FFFF fs2: 8000-FFFF fs3.. etc. In Keil, specify: Off-Chip Code Memory: Eprom: Start: 0x0000, Size: 0x8000 Off-Chip XDATA Memory: Ram: Start: 0x0100, Size: 0x7F00 We are using the same hex file for all the FS and CSB and have no problems until the hex file hits beyon 64K. Any idea what we did wrong and how to fix this problem? Any other question is how do we access the 32 SRAMs? Regards, SD2011-05-17 3:00 AM
See the following post:
Regards, uPSD Applications Engineering